Skip to main content

New Oil for Generator Applications

KOHLER is introducing a new line of aftermarket genuine oil engineered specifically for generator applications. The premium oils are available in three formulationsfor different fuel types and are optimized for use in industrial, mobile, marine, and homegenerators. The fully-synthetic line was specially engineered to help generators run at peak performance, reducing downtime and helping to lower total cost of ownershipcompared with conventional oils used in the same applications.

“Generators have to run when they’re needed –there’s no room for downtime,” said Patricio Iligaray, Manager of Aftermarket Parts for Kohler Power Systems. “And, the oil you choose makes a real difference. Generators are subjected to unique conditions that are different from engines that power other applications. So, it’s important to select an oil –like those in our new line –that are formulated to account for a generator’s temperature, load, idle time, fuel type and more.”

The three new KOHLER oils are engineered to the specific requirements of generators based on the fuel type they use. The company is introducing a 5W-30 formulationfor generators powered by gasoline or gaseous-fueled engines, a 5W-40 formulationfor generators powered by diesel-fueled engines, and a 15W-40 option for generators with gaseous-fueled engines.

Each of the new options is formulated with a synthetic base oil that will maintain critical viscosity while also resisting “burn off,” which can occur with other, lesser quality oils. Special additives in the new KOHLER oil also help protect against engine wear and corrosion, extending overall generator life.

“This is a significant product launch for KOHLER and for our customers” said Vito Minneci, Vice President of Aftermarket Parts and Service for Kohler Power Systems.“The new line of KOHLER premium oil for generator applications provides additional peace-of-mind to our customers and helps them to further protect –and maximize –their investment.”

The new KOHLER generator engine oil can be orderednow in North America and Canada, with some restrictions. It issold in a variety of container sizes to meet the individual needs of generator owners –from 1 quart to 275 gallons, with bulk oil also available.For additional international markets, the aftermarket genuine oil will be part of a phase-two development. To place an order, or to inquire about availability, contact your local KOHLER generator distributor or dealer. A dealer locator can be found online at www.KohlerPower.com.

A global force in power solutions since 1920, Kohler is committed to reliable, leading-edge products and comprehensive after-sale support. Kohler’s acquisition of SDMO in 2005 created one of the world’s largest manufacturers of generators and power solutions. The companies collectively have more than 150 years of experience in industrial power and now benefit from global R&D, manufacturing, and sales and service. For additional information, please visit www.KohlerPower.com or www.KohlerSDMO.com.

About Kohler Co.

Founded in 1873 and headquartered in Kohler, Wisconsin, Kohler Co. is one of America’s oldest and largest privately held companies. With more than 55 manufacturing locations worldwide, Kohler is a global leader in the manufacture of engines and power systems; kitchen and bath products; premier cabinetry and tile; and owner/operator of two of the world’s finest five-star hospitality and golf resort destinations in Kohler and St Andrews, Scotland For more details, please visit KOHLER.com.

Media Inquiries

Erin McMahon
Account Director
erin.mcmahon@publitek.com
+1 630-962-7535