KOHLER’s Most Powerful Generator Set Ever

Kohler Co. is excited to introduce the new KD Series 4500kVA (@50Hz) / 4000kW (@60Hz) diesel powered generator sets – KOHLER’s most powerful generator on the market.
 

Late 2016, KOHLER-SDMO unveiled its all-new range of large diesel industrial generators powered by an entirely new line of KOHLER diesel engines represented by the K135 and K175 engine families. The generators range from 800kVA/800kWe to 3500kVA (@50Hz) / 3250kWe (@60Hz) respectively.
 

Today, based on a strong worldwide market response and an increasing demand on power in mission critical applications, KOHLER-SDMO is proud to officially expand the KD Series with the rollout of four new models ranging up to 4500kVA (@50Hz)/ 4000kWe (@60Hz). Developed by the company’s global team of engineers, these new units incorporate the latest most powerful and sophisticated K175 engine, the KD103V20. This release expands the limits of standby generators and sets KOHLER apart as the most powerful diesel generator set manufacturer in the market.
 

Building on the excellence of the KD Series product line, these generators are designed to deliver extreme durability and ultimate reliability in a variety of emergency and prime applications. The modular design of the KD103V20 powered generator sets deliver unprecedented power density and unrivaled performance. Matched turbochargers are engineered for maximum power and response. High ambient cooling systems ensure performance is maintained in the most extreme environments. Fuel mapping options for either optimized consumption or emissions compliance enable the generators to be deployed globally without worry. Users of the KD Series generators will find cost savings because the line delivers the best fuel consumption at more nodes than any other competitor. KOHLER’s proprietary advanced control and communication system ties the entire system together for a seamless customer experience.
 

When paired with KOHLER’s global sales and support network the KD Series line-up provides leading performance for mission critical and industrial applications. Data centers, healthcare facilities, water utilities, and critical facilities such as airports; can rest assured with a KD Series generator set backed by KOHLER’s Worldwide support network. And when service is needed, KOHLER has a global dealer and distribution infrastructure consisting of more than 800 facilities offering 24/7 parts availability.
 

The new KD Series products will be available for sale in June. For more information, visit kdseries.com and watch the video.

 

About Kohler Power Systems

Kohler Power Systems, a division of Kohler Co., provides complete power systems, including generators (residential, industrial, mobile, portable, and marine), automatic transfer switches, paralleling switchgear, monitoring controls, and accessories for emergency, prime power and energy-management applications. Kohler has delivered energy solutions for markets worldwide since 1920. For more information, visit www.kohlerpower.com.

 

About Kohler Co.

Founded in 1873 and headquartered in Kohler, Wis., Kohler Co. is one of America’s oldest and largest privately held companies comprised of more than 30,000 associates. With more than 50 manufacturing locations worldwide, Kohler is a global leader in the manufacture of kitchen and bath products; engines and power systems; premier furniture, cabinetry and tile; and owner/operator of two of the world’s finest five-star hospitality and golf resort destinations in Kohler and St Andrews, Scotland. For more details, please visit Kohler.com.

Media Inquiries

Erin McMahon
Account Director
erin.mcmahon@publitek.com
+1 630-962-7535
 


kohler-logo

Resilience is Reinvention

Kohler Power Systems is now Rehlko

Follow us on

Products

Parts & Services

DISTRIBUTORS

ABOUT US

HELP