Kohler Launches Three New KD Series Industrial Generators

KOHLER, Wis. – Mar. 13, 2023 – Kohler expands its industry-leading KD Series™ line of industrial generators with two new models, KD700 and KD750 for 60hz markets. These generators feature a new KOHLER 18L advanced diesel engine (KD18L06) that can also run on Hydrotreated Vegetable Oil (HVO) as a renewable fuel source.
These new models join a proven series of gensets that continues to provide the highest power density and best fuel consumption at more nodes than competitors between 700-4000 kW, offering cost savings to users. The new KD units are designed to power mission critical applications, including airports, hospitals, and healthcare facilities, water treatment plants and mid-sized data centers.
The KD700 and KD750 join Kohler’s industrial generators that are engineered to utilize HVO fuel. HVO provides a cleaner and more sustainable alternative to conventional diesel and biofuels. No adaptation is needed and both HVO and diesel can be mixed together. HVO is also highly stable, with no sensitivity to oxidation, so it can be stored long-term. It enables to offset carbon emission by up to 90% by using renewable waste products.
Kohler’s KD Series has proven performance excellence, designed to deliver extreme durability and ultimate reliability in a variety of emergency and prime applications. KD Series generators are engineered to last, with better fuel economy and a small footprint. When paired with Kohler’s global sales and support network the KD Series line-up provides an industry-leading solution that secures customers’ critical operations. And when service is needed, Kohler has a global dealer and distribution infrastructure consisting of more than 800 facilities offering 24/7 parts availability. For additional details about the KOHLER KD Series, please visit www.KohlerPower.com.
Additionally, Kohler announces an upgrade to its KD800 for 50hz markets with the integration of this new KD18L06 engine, coming to market in summer of 2023.
About Kohler Co.
Founded in 1873 and headquartered in Kohler, Wisconsin, Kohler Co. is one of America’s oldest and largest privately held companies, comprised of more than 40,000 associates. Kohler is a global leader in manufacturing kitchen and bath products; engines, generators and clean energy solutions; premier cabinetry, tile and lighting; and owner/operator of two of the world’s finest five-star hospitality and golf resort destinations in Kohler, Wisconsin, and St. Andrews, Scotland. Kohler’s Whistling Straits golf course hosted the 43rd Ryder Cup in 2021. The company also develops solutions to address pressing issues, such as clean water and sanitation, for underserved communities around the world to enhance the quality of life for current and future generations. For more details, please visit kohlercompany.com.
Media Inquiries
Erin McMahon
Account Director
erin.mcmahon@publitek.com
+1 630-962-7535